Simcenter Physical Testing

Simcenter Testlab RT system

Test and experience physical-virtual systems in real-time in the lab or in the office with powerful real-time hardware and software platforms.

Contactez-nous pour savoir comment acheter ce produit dans le pays suivant :
Changer de pays

Simcenter Testlab RT hardware device.

Why Simcenter Testlab RT?

In today’s fast-paced marketplace, businesses face significant challenges such as rapidly evolving customer demands, increasing product complexity and rising development costs. Traditional physical prototyping is no longer sufficient to keep up, especially as the number of product variants grows, making physical testing impractical or impossible. To address these challenges, many businesses are adopting innovative solutions that combine physical and virtual (physical-virtual) systems to test and validate designs in real-time, ensuring seamless interaction between the two domains.

Simcenter Testlab RT helps you test and experience physical-virtual systems in real-time in the lab or in the office with powerful real-time hardware and software platforms.

System-in-the-loop testing – a revolution for vehicle integration

Learn how system-in-the-loop testing de-risks subsystem integration and connects the product development stages by fusing the worlds of simulation and testing.

Integrate the virtual and real systems

Use the X-in-the-loop (XiL) approach to integrate virtual components with physical components for comprehensive system testing.

A holistic approach for testing complex systems

Connect physical test specimens to a virtual system that simulate in real-time to replicate real-world scenarios and minimize integration risks. Quickly adapt to various system configurations and complexities.

Accelerated development

Shift the focus of performance testing from the full physical system to a physical-virtual systems. XiL enables earlier performance evaluation and provides realistic testing in a controlled environment.

Applications for Simcenter Testlab RT

Select...

Early testing of mechatronic systems using physical-virtual integration

Verifying complex products with limited prototypes is difficult. Traditional test benches lack real-world accuracy. With Simcenter physical-virtual testing, you can blend physical rigs and real-time co-simulation, letting you validate and pre-certify subsystems like electric drives or brakes without a full prototype. This method efficiently tests various scenarios and design variants in realistic environments.

Mechatronic systems testing and analysis being performed by an engineer using advanced test bench with dual monitors and control equipment.

Test in real-time

Real-time means that all computations executed by Simcenter Testlab RT are done based on reliable time periods and with microsecond precision. This enables you to accurately combine real-time simulation and real-world physics for systems testing allowing you to virtualize operational environments of the physical system under test (SUT).

Engineers conducting vehicle testing using VR headset and playseat simulator, with one engineer monitoring data on laptop while another operates steering controls in immersive environment.

Connect the real world to the virtual world

Seamlessly interface physical systems and their virtual systems by leveraging analog and digital communication real-time interfaces. You can interface virtual systems to simulators, test bench environments and embedded control units. In addition, gain invaluable insights into system behavior by monitoring, acquiring and analyzing the physical and virtual sensors of the system-under-test in real-time.

Engineer using tablet with AR technology to monitor wind tunnel testing, displaying digital overlay of aerodynamic data on physical aircraft model setup.

Scalable computational performance

Simcenter Testlab RT delivers scalable computational performance, tailored to accommodate the complexity of real-time simulation and control. The real-time environment runs on industrial personal computers (IPCs) via the Siemens SIMATIC® suite, which provide scalable capabilities in terms of central processing unit (CPU) type, memory and disk size and more to best fulfill each application’s needs.

Simcenter Testlab RT hardware devices.

Plug-and-play execution of digital twins

Simplify the process of setting up executable digital twins with an intuitive interface for a plug-and-play experience. With one click, you can upload simulation models, control algorithms, terrains, roads, prerecorded data and more to create a parametrized and real-time executable digital twin. Ensure long-term compatibility with many digital twin formats, such as the Functional Mockup Interface (FMI).

Illustration of a person observing a physical robotic arm on the left and its corresponding digital model on a computer screen on the right.

Achieve faster testing turnaround

Gain remarkable efficiency and flexibility through the ability to swiftly configure and automate tests via an intuitive web interface and by accessing and operating the system remotely from any device. By eliminating complex programming, you can also simplify XiL applications. This helps you minimize downtime, maximize productivity and empowers you to streamline the testing workflow.

Mechatronic systems testing and analysis being performed by an engineer using advanced test bench with dual monitors and control equipment.

Explore Simcenter Testlab RT capabilities

Select...

Real-time co-simulation

Simcenter Testlab RT orchestrates the co-simulation of physical and virtual subsystems in real-time. This is provided in a zero-programming environment. The simulation models that are part of the co-simulation can originate from Siemens solutions (Simcenter Amesim, Simcenter Smart Virtual Sensing) and other vendors. These models must be compatible with real-time and be exported for Simcenter Testlab RT as real-time target. The co-simulation performance is optimized to cover from the simplest use-cases, involving one digital twin and its communication to the real world, to the most advanced use-cases involving multiple digital twins interacting with each other and with multiple physical systems.

real-time-cosimulation-1280x720

Related resources

FAQ