Tune in to this year's annual What's new in Designcenter NX premiere video to learn about all the latest and greatest NX features and enhancements.
We’re always adding new functionality as part of the NX software continuous release cycle, based on innovations from our CAD experts as well as direct feedback from NX users like you.
The June 2025 release of NX sees cloud collaboration, immersive design, and AI-enabled tools as well as some completely new capabilities like NX Inspector and NX DFM Advisor—this is a premiere you won't want to miss.
NX is the heart of Designcenter, the most comprehensive software suite for product development with unmatched scalability, flexibility and functionality.
With four tiers of cloud-based CAD software offerings, Designcenter lets you seamlessly scale from startup to enterprise level and design across both browser and desktop applications with 100% data fidelity.
Unique integrations across the Siemens Xcelerator platform let you collaborate across disciplines and create an end-to-end digital thread for your product from initial concept design through to manufacturing and lifecycle management.
Explore the NX X Design solutions. Built on a common core set of capabilities, NX X Design Essentials, Standard, Advanced and Premium each add functionality to meet the needs of the most demanding design teams.
Each level delivers high-performance CAD capabilities and built-in data management in a cloud-native and SaaS environment. You can use the same data without translation across any level of NX X, and scale your NX X solution as your organization grows.
And NX X is fully interoperable with all other Siemens Xcelerator software and can share data seamlessly to enhance collaboration and accelerate design and production cycles.
Value-based licensing is a flexible, scalable, and cost-effective way to augment your NX capabilities with a wide range of advanced and specialist functionality. While NX X Value Based Licensing is not new in this release, many of the new features and capabilities available in this release are unlocked through token-licensing. With NX X Value Based Licensing, you unlock immediate access to new capabilities as they are released—no additional purchases, licenses or manual updates needed.
Simply purchase a pool of floating NX X Value Based Licensing tokens for your team, and start using a capability in NX to automatically check-out an add-on module for its token value. Once you close NX X or stop using the module, the add-on module is automatically checked back in and the tokens used return to your team's pool.
Have a natural language conversation with Design Copilot NX for advice on using NX software and add-on modules. Powered by generative AI and large language models, the copilot will base its answers on the documentation for the specific version of NX that you’re using.
It will even provide links to the full documentation if you want extra information and you can launch any commands that the copilot mentions direct its responses. Hover over a command to see where it is in the user interface for future reference.
Interact with NX X Copilot intuitively and effortlessly with spoken voice commands. NX Voice really shines for NX Immersive Designer or touchscreen users.
Create, view and edit 3D CAD designs like never before in virtual reality or augmented reality, with full access to the full NX workspace through both physical and virtual monitors.
You can either interact with the model directly with the hand-held controllers or use NX as normal and see your changes update instantly in AR or VR. Seamlessly switch between traditional and immersive engineering with a fully bidirectional extension of NX CAD into the virtual space.
Experience immersive design review at the next level, with NX Immersive Collaborator as you can collaborate in the same virtual reality space with your colleagues.
Start a collaboration session straight from the NX workspace in just a few clicks. A full range of design review tools let you measure, assess and annotate individual parts or entire assemblies.
Explore Immersive Engineering: Designed in exclusive collaboration with Siemens, the Sony XR head-mounted display and controllers are optimized specifically for 3D design.
Dual 4k micro-organic LED (OLED) displays mean unparalleled fidelity when viewing designs. Unique hand controllers allow for precise gesture control alongside mouse and keyboard inputs in hybrid workflows. Meticulous ergonomics let you work comfortably for longer while the flip-up visor allows for seamless multitasking and seamless transitions to and from the immersive experience.
Add model-based characteristics to your product’s digital twin to define downstream quality and manufacturing processes with a groundbreaking new module, NX Inspector. Designcenter is the first CAD-native platform to implement the Digital Metrology Standards Consortium’s Model-Based Characteristics standard.
Automate early manufacturability assessments with the new NX Design for Manufacture (DFM) Advisor. It can analyze your data, identify potential challenges and provide actionable feedback. When you leverage Teamcenter Integration for NX, you can generate reports to share with colleagues and partners, while using the insights to drive additional workflows.
Access fluid flow and thermal simulation capabilities directly within the NX CAD workspace for the first time with NX CFD Designer. This module is a brand-new design simulation tool powered by Simcenter™ FLOEFD technology.
It’s designed to be easy to use for those without CFD experience, with robust automation tackling complex tasks like fluid volume detection and meshing on your behalf. Quickly evaluate a range of operating scenarios and geometry variations at once and compare the results.
Experience peace of mind to sketch more freely and naturally, knowing that NX can take care of geometric precision for you. The new Sketch Checker automatically checks a sketch for common ‘near miss’ issues, such as lines that are not quite parallel or curves that are not quite tangent. Issues appear both in the Graphics Window and the Sketch Navigator and NX can automatically correct issues with a single click.
Explore new commands within NX Realize Shape. The new Blend Curve on Surface and Chamfer Cage commands add even more flexibility to subdivision modeling in NX for creating complex and organic geometry.
Chamfer Cage gives you finer control over transition areas on a design by apply chamfers to the cage controlling a subdivision body. Blend Curve on Surface enables you to edit curves directly on the surface of a subdivision body for a quicker, more intuitive workflow.
Quickly see the impact of your changes as standard parts now update in real time as you set configurations. Design cooling systems better and faster through enhanced cooling channel design with intuitive direct channel creation.
Reduce the risk of failures and improve the quality of finished molded products with mold fill simulation. Mold cost reports are now compatible with more complex mold designs and you can generate detailed design for manufacturing reports to flag potential issues with stakeholders.
Get an even greater level of insight into your products’ performance under a variety of loads. Now, you can run mechanical stress analyses from NX Performance Predictor across entire assemblies as well as individual parts.
NX XはクラウドSaaSのNXであり、3つの拡張可能なシート・オプションを通じてNXのフル機能を提供します。NX Xは、お使いのデバイスに簡単にインストールでき、シームレスな接続が可能です。NXアーキテクチャを基盤としているため、安全なデータ管理機能に自信を持って、データを損失することなく複数の領域にまたがってコラボレーションを継続できます。
購入前に30日間の評価版をダウンロードしてお試しください。