一群人坐在会议桌旁,桌上的笔记本电脑在展示 Simcenter 结构分析

Simcenter

结构分析软件

对结构进行仿真,了解它们在应力、变形等方面的性能。

整合结构分析工具

结构分析仿真旨在研究重量和张力对结构的影响。了解组件或产品装配在应力或振动下的反应对任何行业而言都至关重要。但是,随着产品和材料变得愈发复杂,简单的线性静态分析工具已难以满足工程师们的需求。

Simcenter 提供结构分析软件,可帮助您在单一用户环境中对各种应用进行仿真。您不再需要分别为线性静力学分析、疲劳分析以及非线性分析准备单独的工具。因此,工程部门可以整合结构分析工具,而您只需要了解一个用户界面。

飞机结构设计与分析

从化石燃料动力航空转向可持续航空不仅是一项巨大的工程挑战,也是保持企业竞争力的必由之路。了解互联的机架结构设计和分析方法如何推动可持续航空业的演进。

3D CAE model of a jet engine turbine with cross-sectional view showing internal components and stress analysis visualization.

CAE Summit 2025 with Maya HTT

Meet CAE innovators, experts and developers to get together and share ideas.
October 8-9 | Orlando, FL USA

What is structural analysis software?

Finite element analysis

Finite element analysis (FEA) is the technological and mathematical foundation for simulating structural performance. FEA is a well-established methodology to aid the engineering design and analysis of many kinds of products.

Linear analysis

Linear structural analysis is a method used to determine how a structure behaves under load, assuming a linear elastic material and small deformations. This is the most common type of structural analysis performed today.

Nonlinear analysis

Nonlinear structural analysis is used to account for changes in a structure's geometry, material properties, and stiffness when subjected to loads, where the relationship between forces and displacement is not linear.

Free 30-day trail: Simcenter 3D

Rapidly make a design change that are replicated in your simulation model then simulate again in seconds.

案例分析

Sumitomo Heavy Industries Marine & Engineering

Sumitomo Heavy Industries Marine & Engineering 使用 Simcenter Femap 和 Nastran 进行高质量分析和灵活建模,从而缩短设计时间。

Responding quickly to ship structural analysis needs with easy-to-use Simcenter Femap
Case Study

Responding quickly to ship structural analysis needs with easy-to-use Simcenter Femap

公司:Sumitomo Heavy Industries Marine & Engineering

行业:船舶行业

位置:Yokosuka City , Japan

Siemens 软件:Simcenter 3D Solutions, Simcenter Femap

Explore structural analysis simulation capabilities

Select...

Linear statics analysis

Linear analysis is used to solve static problems, such as determining if a structure will fail under a prescribed load. This analysis is particularly useful for studying structures under static loads, where the loads are applied slowly and remain constant over time.

With the Simcenter Nastran solver, you can simulate both transient and harmonic excitations and use its damping models to choose between direct or forced response.

Simcenter 3D 软件中机械结构线性分析视觉效果图。
Heatmap of the stress points within a car unibody shell

Normal modes

Normal modes analysis helps you to determine the natural frequencies and corresponding mode shapes of a structure. This helps you understand the dynamic behavior of your design and identify potential resonance problems.

Understanding your model's dynamic behavior through modes and test measurements can help you achieve an accurate and efficient solution. Thanks to the rapid analysis capabilities of RDMODES, Simcenter Nastran can generate modes for large systems with numerous modes

Buckling

Simcenter can help you predict the load at which a structure will buckle or undergo a sudden change in shape under compressive loads. This helps you identify potential stability issues and optimize designs for slender or thin-walled structures.

linear buckling of a cylinder in Simcenter 3D

Industry applications

Select...

Simcenter 3D equips aerospace engineers with a robust set of tools for diverse analysis tasks, ensuring the structural integrity, performance, and reliability of aircraft and spacecraft components.

  • Airplane frame analysis: Assesses stiffness, durability, and modal frequency for structural integrity.
  • Wing Evaluation: Measures stiffness, skin buckling resistance, and modal frequency to optimize aerodynamic performance.
  • Control Surfaces Assessment: Evaluates the strength of pylons, ailerons, and stabilizers against flight forces.
  • Spacecraft Durability Checks: Analyzes thermal stress and distortion in composites for reliability in space conditions.
  • Aero Engine Simulation: Provides insights into rotating loads, thermal stress, and components like compressors and turbines.
  • Launch Vehicle Stress Assessment: Evaluates thermal loads, maneuver forces, and wind effects critical for mission success.
Simcenter 3D Structural Analysis Industries Plane

了解结构分析软件产品

点播式在线研讨会 | 51 分钟

船舶结构分析

将仿真和测试相结合,创建真正的数字孪生,确保准确的结构分析仿真。

Simcenter 软件中的船舶结构分析视觉效果图。
Structural analysis

Learn more

Frequently asked questions